Technical FAQs

Ask a Question

What gauge of steel is used for a HOMC16UC or HOMC16UCW load center cover?

Issue:
What gauge of steel is used for a HOMC16UC or HOMC16UCW load center cover?

Product Line:
Homeline Load Center

Environment:
Products sold in North America

Cause:
Need dimension for older Homeline load center

Resolution:
The cover is 16 gauge steel. The door is 18 gauge steel. This cover was 31.06`` H x 15.44`` W. The cover will overlap the load center enclosure by .60`` (19/32``) on all sides. The cover is now obsolete.


CTA-ID : 2006097
Was this helpful?
What can we do to improve the information ?