Technical FAQs

Ask a Question

Can Micrologic ground fault modules be used with 1 & 2 pole breakers in an Iline panel?

1 pole breakers will not accept G shunt trip option, 2 pole breakers have the G shunt trip accessory mounted in the left pole and are 2 poles wide. The GFM100 is three poles wide, and therefore requires 4.5`` of mounting height in an ILINE panel. The additional length of a GFM module requires that the breaker be mounted in a panel able to accept LA breakers.


CTA-ID : 2006093
Was this helpful?
What can we do to improve the information ?