Technical FAQs

Ask a Question

Do QO load centers with copper bus also have copper lugs?

No, the lugs are tin plated aluminum to allow use of either aluminum or copper conductors. No optional copper only lugs are available.

CTA-ID : 2006090
Was this helpful?
What can we do to improve the information ?