Technical FAQs

Ask a Question

Customer trying to order the FAL24025-1212 and it is not a good number. Why not?

The 1212 accessory is a right pole accessory. The two pole breaker has no right pole, only a left pole and a center pole. Use the suffix 1202 for a left pole mounted 1a1b aux. switch accessory. The FAL24025-1202 is a good number.

CTA-ID : 2005879
Was this helpful?
What can we do to improve the information ?