Technical FAQs

Ask a Question

Are optional neutral lugs available to add to a HOM load center neutral assembly?

Yes, optional lug kits are available for installation on Homeline neutral assembly and/or equipment ground bars. Use LK70AN for a #12-2 AWG Aluminum or #14-4 Copper conductor. Use LK100AN for a #6-2/0 Aluminum or Copper conductor. Use LK125AN for a #14-2/0 AWG Aluminum or Copper conductor. Use LK150AN for a #2-3/0 AWG Aluminum or Copper conductor.


CTA-ID : 2005655
Was this helpful?
What can we do to improve the information ?