Technical FAQs

Ask a Question

How does the Class 2510 Type PB1 work?

The panic button allows the toggle operator to be driven to the OFF position with a quick, open-handed stroke requiring no search. The location of the operator is made obvious by a red plastic coating which also provides comfort for the hand.

The panic button kit is easily installed on existing devices in the field. It requires only a screwdriver to fasten the operator with two screws and two washers.

CTA-ID : 2002746
Was this helpful?
What can we do to improve the information ?