Technical FAQs

Ask a Question

What gauge of steel is used for a QOC30UF or QOC30US load center cover?

Issue:
Product Design Features

Product Line:
QO Load centers

Environment:
Gauge of steel

Cause:
Application

Resolution:
The cover is 16 gauge steel. The door is 18 gauge steel.


CTA-ID : 2006081
Was this helpful?
What can we do to improve the information ?