Technical FAQs

Ask a Question

What tenant circuit breakers were used in an EZ4B Vertical EZ Stack device?

The EZ4B used 2-pole, Type QO or Q1 tenant circuit breakers. A QO breaker was used for applications up to 70 ampere. A Q1 breaker was used for 70 through 100 ampere applications.

CTA-ID : 2005860
Was this helpful?
What can we do to improve the information ?