Technical FAQs

Ask a Question

What are the altitude considerations for the ATV28 and any required sizing criteria?

Issue:   What are the altitude considerations for the ATV28 and any required sizing criteria?
 
Product Line:   ATV28
 
Environment:  All
 
Cause:   N/A
 
Resolution:   Up to 3,300 ft (1,000 m) without derating;
derate by 3% for each additional 3,300 ft (1,000 m)


 
Was this helpful?
What can we do to improve the information ?