Technical FAQs

Ask a Question

What is the maximum ambient temperature that the ATV28 can operate at?

Issue: What is the maximum ambient temperature that the ATV28 can operate at?  
 
Product Line:   ATV28
 
Environment:  All
 
Cause:   N/A
 
Resolution:   +14 to +104 F (-10 to +40 C) without grey tape removed
+14 to +122F (-10 to +50C) with grey tape removed


 
Was this helpful?
What can we do to improve the information ?