Technical FAQs

Ask a Question

For the UL Recognized Comb Bus Bar, what is the cross sectional area of the copper on the main bus as well as the tangs that insert into the C60N M9 breaker

Bus cross section: 1.4mm x 8.38mm
Tang cross section: 1.4mm x 4mm
UR file: E65218


CTA-ID : 2005627
Was this helpful?
What can we do to improve the information ?