Technical FAQs

Ask a Question

What is the part number for the door mounted disconnect operator for the ATV58 ECONOFLEX unit?

The part number for the circuit breaker handle is 9421NW3B.

The Econoflex replacement circuit breaker operating handle part number 9421NW3B can only be used as is on the drive units with a GJL breaker. These include 460 VAC drives up to and including 30 HP. This handle is on all the Econoflex drives but it is modified in Seneca when a FAL or a KAL circuit breaker is used. Contact the SquareD Seneca enclosed drives plant for assistance with disconnect handles for drives using FAL or KAL breakers.

CTA-ID : 2005625
Was this helpful?
What can we do to improve the information ?