Technical FAQs

Ask a Question

Are the class 9080 power distribution blocks rated for both ac and dc?

Yes, up to 600 volts. Their current ratings are the same as the wire that they will accept.


CTA-ID : 2006265
Was this helpful?
What can we do to improve the information ?