Technical FAQs

Ask a Question

Can a QO12024L125GWGC, Series S01 load center be top or bottom fed?

Yes. This load center can be mounted with the Main Lugs positioned at the top of the interior for a top feed application. The complete load center can also be rotated 180 degrees to position the Main Lugs at the bottom of the interior for a bottom feed application. No field modifications are required.

CTA-ID : 2006054
Was this helpful?
What can we do to improve the information ?