Technical FAQs

Ask a Question

Can a QO112M100K, Series S01 load center be top or bottom fed?

Yes. This load center can be mounted with the Main Breaker positioned at the top of the interior for a top feed application. The complete load center can also be rotated 180 degrees to position the Main Breaker at the bottom of the interior for a bottom feed application. No field modifications are required.


CTA-ID : 2006047
Was this helpful?
What can we do to improve the information ?