Technical FAQs

Ask a Question

What are the MICROLOGIC Series B Ground Fault Alarm signal terminals?

Terminals  A, B on the wiring diagram correspond to  the following breaker terminals:
LE, ME, NE, PE:   8,9
SE: 21, 22
Terminals for 120 Vac GF push to test correspond to the following breaker terminals:
LE, ME, NE, PE:  3,4
SE: 13,14
For complete details see Data Bulletin 0502DB0001 Ground fault Alarm for LE ME NE PE and SE electronic circuit breakers. URL below.


CTA-ID : 2005840
Was this helpful?
What can we do to improve the information ?