Technical FAQs

Ask a Question

Can a solid state device be used to initiate a 9050JCK timer?

No. The leakage current is enough for the timer to think it is always turned on. The initiating device must have a dry contact. Typically with a solid state input a relay is interposed.


CTA-ID : 2005833
Was this helpful?
What can we do to improve the information ?