Technical FAQs

Ask a Question

What are the dimensions of the 9001BG standard duty control stations?

All 1 and 2 operator units are 3.69`` high, 2.06`` wide, and 2.34`` deep.
All of the 3 operator units are 5.00`` hign, 2.06`` wide, and 2.34`` deep.


CTA-ID : 2005830
Was this helpful?
What can we do to improve the information ?