Technical FAQs

Ask a Question

Is the TVS2EBA12A available in a NEMA 3R enclosure?

Issue:
Is the TVS2EBA12A available in a NEMA 3R enclosure?

Product Line:
Surge protection.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
This unit is rated for NEMA 1/12/3R.


CTA-ID : 2006257
Was this helpful?
What can we do to improve the information ?