Technical FAQs

Ask a Question

What is the Equipment Ground Kit for a HU364DS, Series F05 or F06 Heavy Duty safety switch?

Ground lugs (2) are provided factory installed. The lugs will each accept (1) #14 - 1/0 AWG copper conductor or (1) #12 - 1/0 AWG aluminum conductor.




CTA-ID : 2006243
Was this helpful?
What can we do to improve the information ?