Technical FAQs

Ask a Question

What is the contact material in the ZB4/5 contact blocks?

The material is a silver and nickel alloy. The gold flashed are silver and nickel alloy with a layer of gold.


CTA-ID : 2005825
Was this helpful?
What can we do to improve the information ?