Technical FAQs

Ask a Question

Are equipment ground kits provided factory installed in Heavy Duty safety switches?

Issue:
Selection

Product Line:
HD SS

Cause:
Accessory Selection

Resolution:
In some cases, yes. Kits are included standard in 30 - 200 ampere, Series F5, NEMA Types 4/4X/5 stainless steel and NEMA Type 12 Heavy Duty safety switches. Also included in all NEMA Types of 30 - 200 ampere, Series F5, 4-pole and 6-pole Heavy Duty safety switches.


CTA-ID : 2005824
Was this helpful?
What can we do to improve the information ?