Technical FAQs

Ask a Question

Can an NT and NW be mechanically interlocked using rods or cables?

It is NOT possible to make :
- an interlocking using connecting rods between one Masterpact NT and one Masterpact NW.
- an interlocking using connecting rods between one Masterpact NT FIXED and one Masterpact NT DRAWOUT

It IS possible to make :
- an interlocking using connecting rods between one Masterpact NW FIXED and one Masterpact DRAWOUT.
- an interlocking using cables between one Masterpact NT (fixed or drawout) and one Masterpact NW (fixed or drawout).


CTA-ID : 2005601
Was this helpful?
What can we do to improve the information ?