Technical FAQs

Ask a Question

What type of metal is used to make the Homeline load centers?

Cold rolled steel is used for NEMA 1 load centers. Galvanneal steel is used for NEMA 3R load centers.


CTA-ID : 2006234
Was this helpful?
What can we do to improve the information ?