Technical FAQs

Ask a Question

Can a EZM3600CBU can be converted to a higher ampacity?

No. The nameplate lists the device as 600 amperes maximum. For a higher current rating, the main section should be replaced.


CTA-ID : 2006227
Was this helpful?
What can we do to improve the information ?