Technical FAQs

Ask a Question

Does ANY of the QO Circuit breaker enclosures, QO2100BNF/S, QO2100BNRB, QO2125BNF/S, QO2125NBRB, QO3100BNF/S or QO3100NBRB, include the QO circuit breaker?

Issue:
Product Design Features

Product Line:
QO circuit breaker enclosures

Environment:
Circuit breaker

Cause:
installation

Resolution:
No, the QO circuit breakers must be ordered separately and field installed into the enclosure.


CTA-ID : 2005810
Was this helpful?
What can we do to improve the information ?