Technical FAQs

Ask a Question

What are the repair parts for a SU3040D300L Series M02?

NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only field replaceable parts.
meter cover - 40561-515-01
load center cover - 40561-361-52
Deadfront (interior Trim) - 40561-310-03
load center interior - 40558-425-50
meter base assembly - 62902 (includes 5th jaw)
mounting channel - 40561-420-03
Meter cover sealing screw - X1299 (3-required)
Meter cover mounting screw - 4020513001K
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.


CTA-ID : 2005591
Was this helpful?
What can we do to improve the information ?