Technical FAQs

Ask a Question

What are the repair parts for a CU12L400L Series M03?

NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only field replaceable parts.
Meter Cover - 40562-113-50
Load Center Cover - 40561-361-52
Dead Front Cover - 40561-537-01
Load center interior (breaker base) - 40545-227-50
Meter Base assembly - 62902 (includes 5th jaw)
Mounting Channel - 40561-420-03
Meter cover mounting screws - 21427-202-41 (6-required)
Wing Nuts for mounting meter cover - 23501-020-000 (6-required)
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.


CTA-ID : 2005590
Was this helpful?
What can we do to improve the information ?