Technical FAQs

Ask a Question

What horizontal & vertical bus ampacities are available for the Model 6 LVMCC?

Horizontal bus ampacities available are: 600A, 800A, 1200A, 1600A, 2000A, & 2500A.
Vertical bus ampacities available are:  300A & 600A

Use the document link to the Model 6 Motor Control Center Catalog pg. 15 for more details concerning Bussing Options for Model 6 LVMCC`s.


CTA-ID : 2004643
Was this helpful?
What can we do to improve the information ?