Technical FAQs

Ask a Question

Which enclosures do the XB4 devices use?

Use the XAP enclosures. The XAPA`s are a glass polyester, with available grounding plate, and the XAPG`s are die cast metal.


CTA-ID : 2005361
Was this helpful?
What can we do to improve the information ?