Technical FAQs

Ask a Question

Q1290 Circuit Breaker Replacement

Issue:
What is the replacement for the obsolete Q1290 branch circuit breaker in the obsolete NQO panelboard?

Product Line:
Obsolete NQO panelboards that were sold and supported in the USA.

Environment:
Replacement/maintenance.

Cause:
Are specific branch circuit breakers available for the obsolete NQO panelboards?

Resolution:
Use QO290 can be used in an NQO panel with the SK5669 mounting kit.  


CTA-ID : 3252
Was this helpful?
What can we do to improve the information ?