Technical FAQs

Ask a Question

Can a SC3040M200F be used for an overhead or underground feed application?

Yes, this device is suitable for either overhead or underground feed applications. However, for an overhead application, a Tunnel Kit must be field installed. Order SCTK30 separately.




CTA-ID : 2005347
Was this helpful?
What can we do to improve the information ?