Technical FAQs

Ask a Question

What is the wire range for the main lugs of a 125 ampere convertible Main Lug QO load center?

The main lugs accept (1) #6 - 2/0 AWG aluminum or copper conductors and should be torqued to 50 inch-pounds. The main neutral lugs will accept (1) #4 - 2/0 AWG aluminum or copper conductors and should also be torqued to 50 inch-pounds.


CTA-ID : 2005129
Was this helpful?
What can we do to improve the information ?