Technical FAQs

Ask a Question

Does the Seriplex SPXVME6U1V2 interface card have built-in troubleshooting diagnosics?<br />

Yes, limited and basic diagnosics are available, refer to Design Installation and Troubleshooting guide document number 30298-035-01A ( DIT) appredix B or the SERIPLEX. Interface Card, SPXVME6U1V2, Installation Guide document number 30298-058-01



CTA-ID : 2005119
Was this helpful?
What can we do to improve the information ?