Technical FAQs

Ask a Question

What is the Terminal Lug Data for a H1200SNE4 neutral assembly?

This neutral assembly will accept (8) #3/0 AWG - 750 kcmil copper or aluminum conductors (4 conductors in - 4 conductors out). Two service ground lugs are provided, each will accept (1) #3/0 AWG - 350 kcmil copper or aluminum conductors.


CTA-ID : 2004635
Was this helpful?
What can we do to improve the information ?