Technical FAQs

Ask a Question

Does Seriplex part number 2DS2D2AV2 come in a box or enclosed?<br />Can I purchase only the printed circuit board only?

Yes, it is enclosured in a plastic case, however it is not available in components. 2DS2D2AV2 is a complete unit.

CTA-ID : 2005115
Was this helpful?
What can we do to improve the information ?