Technical FAQs

Ask a Question

Will a QO116M100RB load center accept a QOT tandem or QO tandem circuit breaker?

No, it will not. This is a 16 space/16 circuit panel, accepting full size QO branch breakers only.


CTA-ID : 2005096
Was this helpful?
What can we do to improve the information ?