Technical FAQs

Ask a Question

Will a QO120L125GCK load center accept a QOT tandem or QO tandem circuit breaker?

No, it will not. This is a 20 space/20 circuit panel, accepting full size QO branch breakers only.

CTA-ID : 2005089
Was this helpful?
What can we do to improve the information ?