Technical FAQs

Ask a Question

Is the Q23225NRB suitable for use as service entrance equipment?

Issue:
Application

Product Line:
Circuit Breaker Enclosure

Cause:
Application

Resolution:
Yes, this device is UL Listed and is marked ``SUITABLE FOR USE AS SERVICE EQUIPMENT``.


CTA-ID : 2004841
Was this helpful?
What can we do to improve the information ?