Technical FAQs

Ask a Question

Is the door in a Homeline load center cover hinged from the right or left?

When positioned with the mains located at the top, the door will hinge from the right (open from the left). If the load center in question can be rotated so that the mains are located at the bottom, the door will hinge from the left (open from the right).

CTA-ID : 2004597
Was this helpful?
What can we do to improve the information ?