Technical FAQs

Ask a Question

Is the 9001 KR5R momentary or maintained?

It is momentary. All push buttons are spring return unless specified as maintained or push pull.


CTA-ID : 2005081
Was this helpful?
What can we do to improve the information ?