Technical FAQs

Ask a Question

Will a QO124M100 load center accept a QOT tandem or QO tandem circuit breaker?

No, it will not. This is a 24 space/24 circuit panel, accepting full size QO branch breakers only.

CTA-ID : 2005071
Was this helpful?
What can we do to improve the information ?