Technical FAQs

Ask a Question

Will a QO140M225 load center accept a QOT tandem or QO tandem circuit breaker?

No, it will not. This is a 40 space/40 circuit panel, accepting full size QO branch breakers only.


CTA-ID : 2005057
Was this helpful?
What can we do to improve the information ?