Technical FAQs

Ask a Question

Do any of the Ring Type(MP prefix) Meter-Pak devices include a 5th jaw on the meter socket?

Issue:
Product design features

Product Line:
Meter Pak Metering

Environment:
Meter features

Cause:
Application

Resolution:
No, the Ring type devices are supplied with 4 jaw meter sockets as standard. For field installation of a Fifth Jaw Kit, order catalog number 5J. One kit required per meter socket.


CTA-ID : 2004567
Was this helpful?
What can we do to improve the information ?