Technical FAQs

Ask a Question

What is the torque requirement for a PK15GTA6 Equipment Ground Kit?

The torque required is dependent upon the size of conductor being terminated.
Multi-Terminal Bar:
#14 - 10 CU or #12 - 10 AL = 20 inch pounds
#8 CU or AL = 25 inch pounds
#6 - 4 CU or AL = 35 inch pounds
(2) #14 - 12 CU or (2) #12 -10 AL = 25 inch pounds
I-Beam Bar: #6 - 3/0 CU or AL = 200 inch pounds



CTA-ID : 2005268
Was this helpful?
What can we do to improve the information ?