Technical FAQs

Ask a Question

What is the torque requirement for a PKOGTA6 Equipment Ground Kit?

The torque required is dependent upon the size of conductor being terminated.
Multi-Terminal I-Beam Bar:
#14 - 10 CU or #12 - 10 AL = 35 inch pounds
#8 CU or AL = 40 inch pounds
#6 - 4 CU or AL = 45 inch pounds
#3 - 1/0 CU or AL = 50 inch pounds


CTA-ID : 2005267
Was this helpful?
What can we do to improve the information ?