Technical FAQs

Ask a Question

What is quantity and size of conductors and the torque requirements for the PK23GTAL Equipment Ground Kit?

Issue:
Product features

Product Line:
Load Center Ground Bars

Environment:
Wire range

Cause:
Wire installation

Resolution:
This equipment ground kit has 23 terminals. The terminals provided on the PK23GTAL ground bar will accept the following:
Wire Sizes: 
(1) #14 - #4 CU or AL wire 
(2) #14 CU wires
(2) # 12 CU / AL wires
(2) #10 AL wires 
There is also one large lug terminal capable of terminating (1) #1 - #4/0 copper or aluminum conductor.  

Torque requirements:
Wire range                             Torque LB-IN
(1) #4 CU / AL                            35
(1) #6 CU / AL                            35
(1) #8 CU / AL                            25
(1) #10 - 14 CU, #10 - 12 AL        20 
(2) #14 CU                                 25
(2) #12 CU / AL                          25
(2) #10 AL                                  25
(1) Large box lug #1 - #4/0          200 


SEE THE ATTACHMENT FOR THE DIMENSIONAL INFORMATION FOR THE GROUND BARS.



CTA-ID : 2005264
Was this helpful?
What can we do to improve the information ?