Technical FAQs

Ask a Question

What is the torque requirement for a PK27GTA Equipment Ground Kit?

The torque required is dependent upon the size of conductor being terminated.
Multi-Terminal Bar:
#14 - 10 CU or #12 - 10 AL = 20 inch pounds
#8 CU or AL = 25 inch pounds
#6 - 4 CU or AL = 35 inch pounds
(2) #14 - 12 CU or (2) #12 -10 AL = 25 inch pounds
Large Box Lug - #6 - 2/0 CU or AL = 50 inch pounds


CTA-ID : 2005266
Was this helpful?
What can we do to improve the information ?