Technical FAQs

Ask a Question

Can the catalog number EZML331400 be supplied with a 225 ampere tenant breaker ?

Issue:
Tenant breaker ampere rating

Product Line:
EZM Metering

Environment:
Tenant breaker rating

Cause:
Different ampere rating breakers

Resolution:

Yes, This EZM branch device comes with a LJL type tenant Circuit Breaker that has an adjustable trip setting from 125 Amp to 400 Amp.


CTA-ID : 2005032
Was this helpful?
What can we do to improve the information ?