Technical FAQs

Ask a Question

Can the EZM1600CBU be converted to a 500 ampere trip main breaker device by changing the rating column?

Issue:
Product Design Features

Product Line:
EZM Metering Equipment

Environment:
Main breaker

Cause:
application

Resolution:

No, this device uses a MHP26600 circuit breaker which is fixed trip and there are no rating columns used in this breaker. For this application, you would need to order catalog number EZM1600CBU500. The EZM1600CBU would be supplied with a 500 ampere circuit breaker.


CTA-ID : 2004810
Was this helpful?
What can we do to improve the information ?